MirrorCertificationBuilderLocationType Enumeration

NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.LocationType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderLocationType

class NXOpen.Features.VehicleDesign.MirrorCertificationBuilderLocationType

Bases: object

Used to indicate the mirror location.

Enum Members

Enum Member Enum Member Description
Inside
Represents the inside location
DriverSide
Represents the driver side location
PassengerSide
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.