MirrorCertificationBuilderInstructionFieldsType Enumeration

NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.InstructionFieldsType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInstructionFieldsType

class NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInstructionFieldsType

Bases: object

Used to indicate the shape type of the instruction field.

Enum Members

Enum Member Enum Member Description
Triangle
Represents that the triangle Instruction field will be created
Rectangle
Represents that the rectangle Instruction field will be created
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.