MirrorCertificationBuilderInstructionFieldPositionType Enumeration

NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.InstructionFieldPositionType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInstructionFieldPositionType

class NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInstructionFieldPositionType

Bases: object

Used to indicate the postion where the instruction field will be.

Enum Members

Enum Member Enum Member Description
OnTargetWall
Represents that the instrucition field is on target wall
OnRoadSurface
Represents that the instrucition field is on road surface
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.