MirrorCertificationBuilderInsideStandardsType Enumeration

NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.InsideStandardsType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInsideStandardsType

class NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInsideStandardsType

Bases: object

Used to indicate the standard for the inside mirror.

Enum Members

Enum Member Enum Member Description
UsaCanadaFmvss111Cmvsss111
Represents USA - Canada : FMVSS111 - CMVSSS111 standard
Europe200397EcEcer4602
Represents Europe : 2003/97/EC - ECE R46.02 standard
JapanArticle44Trias29Trias39
Represents Japan : Article 44/TRIAS 29/TRIAS 39 standard
AustraliaAdr1402
Represents Australia : ADR 14/02 standard
SaudiArabiaGulfStatesSsa770771Gs421442
Represents Saudi Arabia - Gulf States : SSA 770/771 GS 421/442 standard
ChinaGb150842006
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.