MirrorCertificationBuilderEyellipsePercentileType Enumeration¶
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.EyellipsePercentileType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyellipsePercentileType
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilderEyellipsePercentileType
¶ Bases:
object
Used to indicate the eyellipse percentile that is used in mirror certification.
Enum Members
Enum Member Enum Member Description Percentile95 Represents 95 Percentile eyellipse will be used for mirror certificationPercentile99 Represents 99 Percentile eyellipse will be used for mirror certification-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-