MirrorCertificationBuilderEyeMethodType Enumeration¶
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.EyeMethodType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyeMethodType
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilderEyeMethodType
¶ Bases:
object
Used to indicate the method to calculate the eye location based on the distance from the eyellipse to the mirror pivot.
Enum Members
Enum Member Enum Member Description MaximumDistance Represents using the maximum distanceMinimumDistance Represents using the minimum distanceMeanDistance Represents using the mean distance-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-