MirrorCertificationBuilderEyeFromOptionType Enumeration

NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.EyeFromOptionType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyeFromOptionType

class NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyeFromOptionType

Bases: object

Used to indicate what part the eye is from.

Enum Members

Enum Member Enum Member Description
WorkPart
Represents eyellipse feature is from work part
RootPart
Represents eyellipse feature is from root part
OtherComponent
Represents eyellipse feature is from the other component Part
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.