HeadImpactUpperRoofDetailBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
HeadImpactUpperRoofDetailBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.VehicleDesign.HeadImpactUpperRoofDetailBuilder
.This is an abstract class and cannot be instantiated.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CreateGeometry | Returns or sets the create construction geometry flag. |
D1 | Returns the calculated horizontal distance between plane A and plane B. |
D2 | Returns the calculated horizontal distance between plane C and plane D. |
PointA | Returns or sets the point A additional geometry. |
PointAFlag | Returns or sets the point A additional geometry flag. |
PointB | Returns or sets the point B additional geometry. |
PointBFlag | Returns or sets the point B additional geometry flag. |
PointC | Returns or sets the point C additional geometry. |
PointCFlag | Returns or sets the point C additional geometry flag. |
PointD | Returns or sets the point D additional geometry. |
PointDFlag | Returns or sets the point D additional geometry flag. |
PointM | Returns or sets the point M alternative point. |
PointMFlag | Returns or sets the point M alternative point flag. |
ReqVerticalMax | Returns the vertical maximum required approach angle. |
ReqVerticalMin | Returns the vertical minimum required approach angle. |
RoofOffset | Returns the offset used to position point C and point D. |
RoofRatio | Returns the ratio used to locate planes E, F, G, and H. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CreateGeometry¶
-
HeadImpactUpperRoofDetailBuilder.
CreateGeometry
¶ Returns or sets the create construction geometry flag.
-------------------------------------
Getter Method
Signature
CreateGeometry()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateGeometry(createGeometry)
Parameters: createGeometry (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
D1¶
-
HeadImpactUpperRoofDetailBuilder.
D1
¶ Returns the calculated horizontal distance between plane A and plane B.
-------------------------------------
Getter Method
Signature
D1()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
D2¶
-
HeadImpactUpperRoofDetailBuilder.
D2
¶ Returns the calculated horizontal distance between plane C and plane D.
-------------------------------------
Getter Method
Signature
D2()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
PointA¶
-
HeadImpactUpperRoofDetailBuilder.
PointA
¶ Returns or sets the point A additional geometry.
-------------------------------------
Getter Method
Signature
PointA()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointA(pointA)
Parameters: pointA ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointAFlag¶
-
HeadImpactUpperRoofDetailBuilder.
PointAFlag
¶ Returns or sets the point A additional geometry flag.
-------------------------------------
Getter Method
Signature
PointAFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointAFlag(pointAFlag)
Parameters: pointAFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointB¶
-
HeadImpactUpperRoofDetailBuilder.
PointB
¶ Returns or sets the point B additional geometry.
-------------------------------------
Getter Method
Signature
PointB()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointB(pointB)
Parameters: pointB ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointBFlag¶
-
HeadImpactUpperRoofDetailBuilder.
PointBFlag
¶ Returns or sets the point B additional geometry flag.
-------------------------------------
Getter Method
Signature
PointBFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointBFlag(pointBFlag)
Parameters: pointBFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointC¶
-
HeadImpactUpperRoofDetailBuilder.
PointC
¶ Returns or sets the point C additional geometry.
-------------------------------------
Getter Method
Signature
PointC()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointC(pointC)
Parameters: pointC ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointCFlag¶
-
HeadImpactUpperRoofDetailBuilder.
PointCFlag
¶ Returns or sets the point C additional geometry flag.
-------------------------------------
Getter Method
Signature
PointCFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointCFlag(pointCFlag)
Parameters: pointCFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointD¶
-
HeadImpactUpperRoofDetailBuilder.
PointD
¶ Returns or sets the point D additional geometry.
-------------------------------------
Getter Method
Signature
PointD()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointD(pointD)
Parameters: pointD ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointDFlag¶
-
HeadImpactUpperRoofDetailBuilder.
PointDFlag
¶ Returns or sets the point D additional geometry flag.
-------------------------------------
Getter Method
Signature
PointDFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointDFlag(pointDFlag)
Parameters: pointDFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointM¶
-
HeadImpactUpperRoofDetailBuilder.
PointM
¶ Returns or sets the point M alternative point.
-------------------------------------
Getter Method
Signature
PointM()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointM(pointM)
Parameters: pointM ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointMFlag¶
-
HeadImpactUpperRoofDetailBuilder.
PointMFlag
¶ Returns or sets the point M alternative point flag.
-------------------------------------
Getter Method
Signature
PointMFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointMFlag(pointMFlag)
Parameters: pointMFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ReqVerticalMax¶
-
HeadImpactUpperRoofDetailBuilder.
ReqVerticalMax
¶ Returns the vertical maximum required approach angle.
-------------------------------------
Getter Method
Signature
ReqVerticalMax()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReqVerticalMin¶
-
HeadImpactUpperRoofDetailBuilder.
ReqVerticalMin
¶ Returns the vertical minimum required approach angle.
-------------------------------------
Getter Method
Signature
ReqVerticalMin()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
RoofOffset¶
-
HeadImpactUpperRoofDetailBuilder.
RoofOffset
¶ Returns the offset used to position point C and point D.
-------------------------------------
Getter Method
Signature
RoofOffset()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
RoofRatio¶
-
HeadImpactUpperRoofDetailBuilder.
RoofRatio
¶ Returns the ratio used to locate planes E, F, G, and H.
-------------------------------------
Getter Method
Signature
RoofRatio()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
HeadImpactUpperRoofDetailBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.