HeadImpactSideRailWizardBuilder Class

class NXOpen.Features.VehicleDesign.HeadImpactSideRailWizardBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Features.VehicleDesign.HeadImpactSideRailWizardBuilder.

This is an abstract class and cannot be instantiated.

New in version NX9.0.0.

Properties

Property Description
DaylightOpeningLeft Returns the left forward daylight opening geometry.
DaylightOpeningRight Returns the right forward daylight opening geometry.
DoorOpeningLeft Returns the left forward door opening geometry.
DoorOpeningRight Returns the right forward door opening geometry.
Tag Returns the Tag for this object.
UpperRoofInterior Returns the upper roof interior geometry.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

DaylightOpeningLeft

HeadImpactSideRailWizardBuilder.DaylightOpeningLeft

Returns the left forward daylight opening geometry.

-------------------------------------

Getter Method

Signature DaylightOpeningLeft()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

DaylightOpeningRight

HeadImpactSideRailWizardBuilder.DaylightOpeningRight

Returns the right forward daylight opening geometry.

-------------------------------------

Getter Method

Signature DaylightOpeningRight()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

DoorOpeningLeft

HeadImpactSideRailWizardBuilder.DoorOpeningLeft

Returns the left forward door opening geometry.

-------------------------------------

Getter Method

Signature DoorOpeningLeft()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

DoorOpeningRight

HeadImpactSideRailWizardBuilder.DoorOpeningRight

Returns the right forward door opening geometry.

-------------------------------------

Getter Method

Signature DoorOpeningRight()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

UpperRoofInterior

HeadImpactSideRailWizardBuilder.UpperRoofInterior

Returns the upper roof interior geometry.

-------------------------------------

Getter Method

Signature UpperRoofInterior()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

Method Detail

Validate

HeadImpactSideRailWizardBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.