HeadImpactSideRailDetailBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
HeadImpactSideRailDetailBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder
.This is an abstract class and cannot be instantiated.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CreateGeometry | Returns or sets the create construction geometry flag. |
PT11Left | Returns or sets the left PT11 additional geometry. |
PT11LeftFlag | Returns or sets the left PT11 additional geometry flag. |
PT11Right | Returns or sets the right PT11 additional geometry. |
PT11RightFlag | Returns or sets the right PT11 additional geometry flag. |
PT12Left | Returns or sets the left PT12 additional geometry. |
PT12LeftFlag | Returns or sets the left PT12 additional geometry flag. |
PT12Right | Returns or sets the right PT12 additional geometry. |
PT12RightFlag | Returns or sets the right PT12 additional geometry flag. |
PT14Left | Returns or sets the left PT14 additional geometry. |
PT14LeftFlag | Returns or sets the left PT14 additional geometry flag. |
PT14Right | Returns or sets the right PT14 additional geometry. |
PT14RightFlag | Returns or sets the right PT14 additional geometry flag. |
ReqHorizontalLeftExact | Returns the left horizontal required approach angle. |
ReqHorizontalRightExact | Returns the right horizontal required approach angle. |
ReqVerticalMax | Returns the vertical maximum required approach angle. |
ReqVerticalMin | Returns the vertical minimum required approach angle. |
SR1Left | Returns or sets the left SR1 alternative point. |
SR1LeftFlag | Returns or sets the left SR1 alternative point flag. |
SR1Offset | Returns the offset used to position SR1. |
SR1Right | Returns or sets the right SR1 alternative point. |
SR1RightFlag | Returns or sets the right SR1 alternative point flag. |
SR2ALeft | Returns or sets the left SR2A alternative point. |
SR2ALeftFlag | Returns or sets the left SR2A alternative point flag. |
SR2ARight | Returns or sets the right SR2A alternative point. |
SR2ARightFlag | Returns or sets the right SR2A alternative point flag. |
SR2BLeft | Returns or sets the left SR2B alternative point. |
SR2BLeftFlag | Returns or sets the left SR2B alternative point flag. |
SR2BRight | Returns or sets the right SR2B alternative point. |
SR2BRightFlag | Returns or sets the right SR2B alternative point flag. |
SR2Left | Returns or sets the left SR2 alternative point. |
SR2LeftFlag | Returns or sets the left SR2 alternative point flag. |
SR2Offset | Returns the offset used to position SR2. |
SR2Right | Returns or sets the right SR2 alternative point. |
SR2RightFlag | Returns or sets the right SR2 alternative point flag. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CreateGeometry¶
-
HeadImpactSideRailDetailBuilder.
CreateGeometry
¶ Returns or sets the create construction geometry flag.
-------------------------------------
Getter Method
Signature
CreateGeometry()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateGeometry(createGeometry)
Parameters: createGeometry (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT11Left¶
-
HeadImpactSideRailDetailBuilder.
PT11Left
¶ Returns or sets the left PT11 additional geometry.
-------------------------------------
Getter Method
Signature
PT11Left()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT11Left(pt11Left)
Parameters: pt11Left ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT11LeftFlag¶
-
HeadImpactSideRailDetailBuilder.
PT11LeftFlag
¶ Returns or sets the left PT11 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT11LeftFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT11LeftFlag(pt11LeftFlag)
Parameters: pt11LeftFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT11Right¶
-
HeadImpactSideRailDetailBuilder.
PT11Right
¶ Returns or sets the right PT11 additional geometry.
-------------------------------------
Getter Method
Signature
PT11Right()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT11Right(pt11Right)
Parameters: pt11Right ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT11RightFlag¶
-
HeadImpactSideRailDetailBuilder.
PT11RightFlag
¶ Returns or sets the right PT11 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT11RightFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT11RightFlag(pt11RightFlag)
Parameters: pt11RightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT12Left¶
-
HeadImpactSideRailDetailBuilder.
PT12Left
¶ Returns or sets the left PT12 additional geometry.
-------------------------------------
Getter Method
Signature
PT12Left()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT12Left(pt12Left)
Parameters: pt12Left ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT12LeftFlag¶
-
HeadImpactSideRailDetailBuilder.
PT12LeftFlag
¶ Returns or sets the left PT12 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT12LeftFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT12LeftFlag(pt12LeftFlag)
Parameters: pt12LeftFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT12Right¶
-
HeadImpactSideRailDetailBuilder.
PT12Right
¶ Returns or sets the right PT12 additional geometry.
-------------------------------------
Getter Method
Signature
PT12Right()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT12Right(pt12Right)
Parameters: pt12Right ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT12RightFlag¶
-
HeadImpactSideRailDetailBuilder.
PT12RightFlag
¶ Returns or sets the right PT12 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT12RightFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT12RightFlag(pt12RightFlag)
Parameters: pt12RightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT14Left¶
-
HeadImpactSideRailDetailBuilder.
PT14Left
¶ Returns or sets the left PT14 additional geometry.
-------------------------------------
Getter Method
Signature
PT14Left()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT14Left(pt14Left)
Parameters: pt14Left ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT14LeftFlag¶
-
HeadImpactSideRailDetailBuilder.
PT14LeftFlag
¶ Returns or sets the left PT14 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT14LeftFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT14LeftFlag(pt14LeftFlag)
Parameters: pt14LeftFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT14Right¶
-
HeadImpactSideRailDetailBuilder.
PT14Right
¶ Returns or sets the right PT14 additional geometry.
-------------------------------------
Getter Method
Signature
PT14Right()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT14Right(pt14Right)
Parameters: pt14Right ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT14RightFlag¶
-
HeadImpactSideRailDetailBuilder.
PT14RightFlag
¶ Returns or sets the right PT14 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT14RightFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT14RightFlag(pt14RightFlag)
Parameters: pt14RightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ReqHorizontalLeftExact¶
-
HeadImpactSideRailDetailBuilder.
ReqHorizontalLeftExact
¶ Returns the left horizontal required approach angle.
-------------------------------------
Getter Method
Signature
ReqHorizontalLeftExact()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReqHorizontalRightExact¶
-
HeadImpactSideRailDetailBuilder.
ReqHorizontalRightExact
¶ Returns the right horizontal required approach angle.
-------------------------------------
Getter Method
Signature
ReqHorizontalRightExact()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReqVerticalMax¶
-
HeadImpactSideRailDetailBuilder.
ReqVerticalMax
¶ Returns the vertical maximum required approach angle.
-------------------------------------
Getter Method
Signature
ReqVerticalMax()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReqVerticalMin¶
-
HeadImpactSideRailDetailBuilder.
ReqVerticalMin
¶ Returns the vertical minimum required approach angle.
-------------------------------------
Getter Method
Signature
ReqVerticalMin()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
SR1Left¶
-
HeadImpactSideRailDetailBuilder.
SR1Left
¶ Returns or sets the left SR1 alternative point.
-------------------------------------
Getter Method
Signature
SR1Left()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR1Left(sr1Left)
Parameters: sr1Left ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR1LeftFlag¶
-
HeadImpactSideRailDetailBuilder.
SR1LeftFlag
¶ Returns or sets the left SR1 alternative point flag.
-------------------------------------
Getter Method
Signature
SR1LeftFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR1LeftFlag(sr1LeftFlag)
Parameters: sr1LeftFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR1Offset¶
-
HeadImpactSideRailDetailBuilder.
SR1Offset
¶ Returns the offset used to position SR1.
-------------------------------------
Getter Method
Signature
SR1Offset()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
SR1Right¶
-
HeadImpactSideRailDetailBuilder.
SR1Right
¶ Returns or sets the right SR1 alternative point.
-------------------------------------
Getter Method
Signature
SR1Right()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR1Right(sr1Right)
Parameters: sr1Right ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR1RightFlag¶
-
HeadImpactSideRailDetailBuilder.
SR1RightFlag
¶ Returns or sets the right SR1 alternative point flag.
-------------------------------------
Getter Method
Signature
SR1RightFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR1RightFlag(sr1RightFlag)
Parameters: sr1RightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2ALeft¶
-
HeadImpactSideRailDetailBuilder.
SR2ALeft
¶ Returns or sets the left SR2A alternative point.
-------------------------------------
Getter Method
Signature
SR2ALeft()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2ALeft(sr2aLeft)
Parameters: sr2aLeft ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2ALeftFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2ALeftFlag
¶ Returns or sets the left SR2A alternative point flag.
-------------------------------------
Getter Method
Signature
SR2ALeftFlag()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2ALeftFlag(sr2aLeftFlag)
Parameters: sr2aLeftFlag (bool) – New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2ARight¶
-
HeadImpactSideRailDetailBuilder.
SR2ARight
¶ Returns or sets the right SR2A alternative point.
-------------------------------------
Getter Method
Signature
SR2ARight()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2ARight(sr2aRight)
Parameters: sr2aRight ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2ARightFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2ARightFlag
¶ Returns or sets the right SR2A alternative point flag.
-------------------------------------
Getter Method
Signature
SR2ARightFlag()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2ARightFlag(sr2aRightFlag)
Parameters: sr2aRightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2BLeft¶
-
HeadImpactSideRailDetailBuilder.
SR2BLeft
¶ Returns or sets the left SR2B alternative point.
-------------------------------------
Getter Method
Signature
SR2BLeft()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2BLeft(sr2bLeft)
Parameters: sr2bLeft ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2BLeftFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2BLeftFlag
¶ Returns or sets the left SR2B alternative point flag.
-------------------------------------
Getter Method
Signature
SR2BLeftFlag()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2BLeftFlag(sr2bLeftFlag)
Parameters: sr2bLeftFlag (bool) – New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2BRight¶
-
HeadImpactSideRailDetailBuilder.
SR2BRight
¶ Returns or sets the right SR2B alternative point.
-------------------------------------
Getter Method
Signature
SR2BRight()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2BRight(sr2bRight)
Parameters: sr2bRight ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2BRightFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2BRightFlag
¶ Returns or sets the right SR2B alternative point flag.
-------------------------------------
Getter Method
Signature
SR2BRightFlag()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2BRightFlag(sr2bRightFlag)
Parameters: sr2bRightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2Left¶
-
HeadImpactSideRailDetailBuilder.
SR2Left
¶ Returns or sets the left SR2 alternative point.
-------------------------------------
Getter Method
Signature
SR2Left()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ALeft()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SR2Left(sr2Left)
Parameters: sr2Left ( NXOpen.Point
) –New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ALeft()
instead.License requirements: nx_general_packaging (“NX General Packaging”)
SR2LeftFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2LeftFlag
¶ Returns or sets the left SR2 alternative point flag.
-------------------------------------
Getter Method
Signature
SR2LeftFlag()
Returns: Return type: bool New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ALeftFlag()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SR2LeftFlag(sr2LeftFlag)
Parameters: sr2LeftFlag (bool) – New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ALeftFlag()
instead.License requirements: nx_general_packaging (“NX General Packaging”)
SR2Offset¶
-
HeadImpactSideRailDetailBuilder.
SR2Offset
¶ Returns the offset used to position SR2.
-------------------------------------
Getter Method
Signature
SR2Offset()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
SR2Right¶
-
HeadImpactSideRailDetailBuilder.
SR2Right
¶ Returns or sets the right SR2 alternative point.
-------------------------------------
Getter Method
Signature
SR2Right()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ARight()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SR2Right(sr2Right)
Parameters: sr2Right ( NXOpen.Point
) –New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ARight()
instead.License requirements: nx_general_packaging (“NX General Packaging”)
SR2RightFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2RightFlag
¶ Returns or sets the right SR2 alternative point flag.
-------------------------------------
Getter Method
Signature
SR2RightFlag()
Returns: Return type: bool New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ARightFlag()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SR2RightFlag(sr2RightFlag)
Parameters: sr2RightFlag (bool) – New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ARightFlag()
instead.License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
HeadImpactSideRailDetailBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.