HeadImpactRearHeaderDetailBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
HeadImpactRearHeaderDetailBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.VehicleDesign.HeadImpactRearHeaderDetailBuilder
.This is an abstract class and cannot be instantiated.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CreateGeometry | Returns or sets the create construction geometry flag. |
RHLeft | Returns or sets the left rear header target alternative point. |
RHLeftFlag | Returns or sets the left rear header target alternative point flag. |
RHOffsetMax | Returns the maximum offset allowed to position the rear header target. |
RHRight | Returns or sets the right rear header target alternative point. |
RHRightFlag | Returns or sets the right rear header target alternative point flag. |
ReqHorizontalExact | Returns the horizontal exact required approach angle. |
ReqVerticalMax | Returns the vertical maximum required approach angle. |
ReqVerticalMin | Returns the vertical minimum required approach angle. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CreateGeometry¶
-
HeadImpactRearHeaderDetailBuilder.
CreateGeometry
¶ Returns or sets the create construction geometry flag.
-------------------------------------
Getter Method
Signature
CreateGeometry()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateGeometry(createGeometry)
Parameters: createGeometry (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RHLeft¶
-
HeadImpactRearHeaderDetailBuilder.
RHLeft
¶ Returns or sets the left rear header target alternative point.
-------------------------------------
Getter Method
Signature
RHLeft()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RHLeft(rhLeft)
Parameters: rhLeft ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RHLeftFlag¶
-
HeadImpactRearHeaderDetailBuilder.
RHLeftFlag
¶ Returns or sets the left rear header target alternative point flag.
-------------------------------------
Getter Method
Signature
RHLeftFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RHLeftFlag(rhLeftFlag)
Parameters: rhLeftFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RHOffsetMax¶
-
HeadImpactRearHeaderDetailBuilder.
RHOffsetMax
¶ Returns the maximum offset allowed to position the rear header target.
-------------------------------------
Getter Method
Signature
RHOffsetMax()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
RHRight¶
-
HeadImpactRearHeaderDetailBuilder.
RHRight
¶ Returns or sets the right rear header target alternative point.
-------------------------------------
Getter Method
Signature
RHRight()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RHRight(rhRight)
Parameters: rhRight ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RHRightFlag¶
-
HeadImpactRearHeaderDetailBuilder.
RHRightFlag
¶ Returns or sets the right rear header target alternative point flag.
-------------------------------------
Getter Method
Signature
RHRightFlag()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RHRightFlag(rhRightFlag)
Parameters: rhRightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ReqHorizontalExact¶
-
HeadImpactRearHeaderDetailBuilder.
ReqHorizontalExact
¶ Returns the horizontal exact required approach angle.
-------------------------------------
Getter Method
Signature
ReqHorizontalExact()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReqVerticalMax¶
-
HeadImpactRearHeaderDetailBuilder.
ReqVerticalMax
¶ Returns the vertical maximum required approach angle.
-------------------------------------
Getter Method
Signature
ReqVerticalMax()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReqVerticalMin¶
-
HeadImpactRearHeaderDetailBuilder.
ReqVerticalMin
¶ Returns the vertical minimum required approach angle.
-------------------------------------
Getter Method
Signature
ReqVerticalMin()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
HeadImpactRearHeaderDetailBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.