HeadImpactFrontHeaderDetailBuilder Class

class NXOpen.Features.VehicleDesign.HeadImpactFrontHeaderDetailBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Features.VehicleDesign.HeadImpactFrontHeaderDetailBuilder.

This is an abstract class and cannot be instantiated.

New in version NX9.0.0.

Properties

Property Description
CreateGeometry Returns or sets the create construction geometry flag.
FH1Left Returns or sets the left FH1 alternative point.
FH1LeftFlag Returns or sets the left FH1 alternative point flag.
FH1Offset Returns the offset used to position FH1.
FH1Right Returns or sets the right FH1 alternative point.
FH1RightFlag Returns or sets the right FH1 alternative point flag.
FH2Left Returns or sets the left FH2 alternative point.
FH2LeftFlag Returns or sets the left FH2 alternative point flag.
FH2Offset Returns the offset used to position FH2.
FH2Right Returns or sets the right FH2 alternative point.
FH2RightFlag Returns or sets the right FH2 alternative point flag.
ReqHorizontalExact Returns the horizontal exact required approach angle.
ReqVerticalMax Returns the vertical maximum required approach angle.
ReqVerticalMin Returns the vertical minimum required approach angle.
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

CreateGeometry

HeadImpactFrontHeaderDetailBuilder.CreateGeometry

Returns or sets the create construction geometry flag.

-------------------------------------

Getter Method

Signature CreateGeometry()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CreateGeometry(createGeometry)

Parameters:createGeometry (bool) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

FH1Left

HeadImpactFrontHeaderDetailBuilder.FH1Left

Returns or sets the left FH1 alternative point.

-------------------------------------

Getter Method

Signature FH1Left()

Returns:
Return type:NXOpen.Point

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FH1Left(fh1Left)

Parameters:fh1Left (NXOpen.Point) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

FH1LeftFlag

HeadImpactFrontHeaderDetailBuilder.FH1LeftFlag

Returns or sets the left FH1 alternative point flag.

-------------------------------------

Getter Method

Signature FH1LeftFlag()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FH1LeftFlag(fh1LeftFlag)

Parameters:fh1LeftFlag (bool) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

FH1Offset

HeadImpactFrontHeaderDetailBuilder.FH1Offset

Returns the offset used to position FH1.

-------------------------------------

Getter Method

Signature FH1Offset()

Returns:
Return type:NXOpen.Expression

New in version NX9.0.0.

License requirements: None.

FH1Right

HeadImpactFrontHeaderDetailBuilder.FH1Right

Returns or sets the right FH1 alternative point.

-------------------------------------

Getter Method

Signature FH1Right()

Returns:
Return type:NXOpen.Point

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FH1Right(fh1Right)

Parameters:fh1Right (NXOpen.Point) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

FH1RightFlag

HeadImpactFrontHeaderDetailBuilder.FH1RightFlag

Returns or sets the right FH1 alternative point flag.

-------------------------------------

Getter Method

Signature FH1RightFlag()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FH1RightFlag(fh1RightFlag)

Parameters:fh1RightFlag (bool) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

FH2Left

HeadImpactFrontHeaderDetailBuilder.FH2Left

Returns or sets the left FH2 alternative point.

-------------------------------------

Getter Method

Signature FH2Left()

Returns:
Return type:NXOpen.Point

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FH2Left(rp2Left)

Parameters:rp2Left (NXOpen.Point) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

FH2LeftFlag

HeadImpactFrontHeaderDetailBuilder.FH2LeftFlag

Returns or sets the left FH2 alternative point flag.

-------------------------------------

Getter Method

Signature FH2LeftFlag()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FH2LeftFlag(rp2LeftFlag)

Parameters:rp2LeftFlag (bool) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

FH2Offset

HeadImpactFrontHeaderDetailBuilder.FH2Offset

Returns the offset used to position FH2.

-------------------------------------

Getter Method

Signature FH2Offset()

Returns:
Return type:NXOpen.Expression

New in version NX9.0.0.

License requirements: None.

FH2Right

HeadImpactFrontHeaderDetailBuilder.FH2Right

Returns or sets the right FH2 alternative point.

-------------------------------------

Getter Method

Signature FH2Right()

Returns:
Return type:NXOpen.Point

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FH2Right(rp2Right)

Parameters:rp2Right (NXOpen.Point) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

FH2RightFlag

HeadImpactFrontHeaderDetailBuilder.FH2RightFlag

Returns or sets the right FH2 alternative point flag.

-------------------------------------

Getter Method

Signature FH2RightFlag()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FH2RightFlag(rp2RightFlag)

Parameters:rp2RightFlag (bool) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

ReqHorizontalExact

HeadImpactFrontHeaderDetailBuilder.ReqHorizontalExact

Returns the horizontal exact required approach angle.

-------------------------------------

Getter Method

Signature ReqHorizontalExact()

Returns:
Return type:NXOpen.Expression

New in version NX9.0.0.

License requirements: None.

ReqVerticalMax

HeadImpactFrontHeaderDetailBuilder.ReqVerticalMax

Returns the vertical maximum required approach angle.

-------------------------------------

Getter Method

Signature ReqVerticalMax()

Returns:
Return type:NXOpen.Expression

New in version NX9.0.0.

License requirements: None.

ReqVerticalMin

HeadImpactFrontHeaderDetailBuilder.ReqVerticalMin

Returns the vertical minimum required approach angle.

-------------------------------------

Getter Method

Signature ReqVerticalMin()

Returns:
Return type:NXOpen.Expression

New in version NX9.0.0.

License requirements: None.

Method Detail

Validate

HeadImpactFrontHeaderDetailBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.