HeadImpactBPillarWizardBuilder Class

class NXOpen.Features.VehicleDesign.HeadImpactBPillarWizardBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Features.VehicleDesign.HeadImpactBPillarWizardBuilder.

This is an abstract class and cannot be instantiated.

New in version NX9.0.0.

Properties

Property Description
BP2Left Returns or sets the left B-pillar 2 point.
BP2Right Returns or sets the right B-pillar 2 point.
BPillarLeft Returns the left B pillar geometry.
BPillarRight Returns the right B pillar geometry.
CenterlineLeft Returns the left B Pillar centerline geometry.
CenterlineRight Returns the right B Pillar centerline geometry.
DaylightBottomLeft Returns or sets the left daylight opening bottom point.
DaylightBottomRight Returns or sets the right daylight opening bottom point.
DaylightOpeningLeft Returns the left forward daylight opening geometry.
DaylightOpeningRight Returns the right forward daylight opening geometry.
DoorOpeningLeft Returns the left forward door opening geometry.
DoorOpeningRight Returns the right forward door opening geometry.
DoorTopLeft Returns or sets the left door opening top point.
DoorTopRight Returns or sets the right door opening top point.
Tag Returns the Tag for this object.
UpperRoofInterior Returns the upper roof interior geometry.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

BP2Left

HeadImpactBPillarWizardBuilder.BP2Left

Returns or sets the left B-pillar 2 point.

-------------------------------------

Getter Method

Signature BP2Left()

Returns:
Return type:NXOpen.Point

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature BP2Left(bp2Left)

Parameters:bp2Left (NXOpen.Point) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

BP2Right

HeadImpactBPillarWizardBuilder.BP2Right

Returns or sets the right B-pillar 2 point.

-------------------------------------

Getter Method

Signature BP2Right()

Returns:
Return type:NXOpen.Point

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature BP2Right(bp2Right)

Parameters:bp2Right (NXOpen.Point) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

BPillarLeft

HeadImpactBPillarWizardBuilder.BPillarLeft

Returns the left B pillar geometry.

-------------------------------------

Getter Method

Signature BPillarLeft()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

BPillarRight

HeadImpactBPillarWizardBuilder.BPillarRight

Returns the right B pillar geometry.

-------------------------------------

Getter Method

Signature BPillarRight()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

CenterlineLeft

HeadImpactBPillarWizardBuilder.CenterlineLeft

Returns the left B Pillar centerline geometry.

-------------------------------------

Getter Method

Signature CenterlineLeft()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

CenterlineRight

HeadImpactBPillarWizardBuilder.CenterlineRight

Returns the right B Pillar centerline geometry.

-------------------------------------

Getter Method

Signature CenterlineRight()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

DaylightBottomLeft

HeadImpactBPillarWizardBuilder.DaylightBottomLeft

Returns or sets the left daylight opening bottom point.

-------------------------------------

Getter Method

Signature DaylightBottomLeft()

Returns:
Return type:NXOpen.Point

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DaylightBottomLeft(daylightBottomLeft)

Parameters:daylightBottomLeft (NXOpen.Point) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

DaylightBottomRight

HeadImpactBPillarWizardBuilder.DaylightBottomRight

Returns or sets the right daylight opening bottom point.

-------------------------------------

Getter Method

Signature DaylightBottomRight()

Returns:
Return type:NXOpen.Point

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DaylightBottomRight(daylightBottomRight)

Parameters:daylightBottomRight (NXOpen.Point) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

DaylightOpeningLeft

HeadImpactBPillarWizardBuilder.DaylightOpeningLeft

Returns the left forward daylight opening geometry.

-------------------------------------

Getter Method

Signature DaylightOpeningLeft()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

DaylightOpeningRight

HeadImpactBPillarWizardBuilder.DaylightOpeningRight

Returns the right forward daylight opening geometry.

-------------------------------------

Getter Method

Signature DaylightOpeningRight()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

DoorOpeningLeft

HeadImpactBPillarWizardBuilder.DoorOpeningLeft

Returns the left forward door opening geometry.

-------------------------------------

Getter Method

Signature DoorOpeningLeft()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

DoorOpeningRight

HeadImpactBPillarWizardBuilder.DoorOpeningRight

Returns the right forward door opening geometry.

-------------------------------------

Getter Method

Signature DoorOpeningRight()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

DoorTopLeft

HeadImpactBPillarWizardBuilder.DoorTopLeft

Returns or sets the left door opening top point.

-------------------------------------

Getter Method

Signature DoorTopLeft()

Returns:
Return type:NXOpen.Point

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DoorTopLeft(doorTopLeft)

Parameters:doorTopLeft (NXOpen.Point) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

DoorTopRight

HeadImpactBPillarWizardBuilder.DoorTopRight

Returns or sets the right door opening top point.

-------------------------------------

Getter Method

Signature DoorTopRight()

Returns:
Return type:NXOpen.Point

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DoorTopRight(doorTopRight)

Parameters:doorTopRight (NXOpen.Point) –

New in version NX9.0.0.

License requirements: nx_general_packaging (“NX General Packaging”)

UpperRoofInterior

HeadImpactBPillarWizardBuilder.UpperRoofInterior

Returns the upper roof interior geometry.

-------------------------------------

Getter Method

Signature UpperRoofInterior()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

Method Detail

Validate

HeadImpactBPillarWizardBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.