CrashBarrierBuilderShapeType Enumeration

NXOpen.Features.VehicleDesign.CrashBarrierBuilder.ShapeType is an alias for NXOpen.Features.VehicleDesign.CrashBarrierBuilderShapeType

class NXOpen.Features.VehicleDesign.CrashBarrierBuilderShapeType

Bases: object

Represents the shape types.

Enum Members

Enum Member Enum Member Description
RCAR2004Front
RCAR2004Rear
Rcar2006
Iihs2009
IIHS2009MultiDomain
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.