CrashBarrierBuilderCrossPositionType Enumeration

NXOpen.Features.VehicleDesign.CrashBarrierBuilder.CrossPositionType is an alias for NXOpen.Features.VehicleDesign.CrashBarrierBuilderCrossPositionType

class NXOpen.Features.VehicleDesign.CrashBarrierBuilderCrossPositionType

Bases: object

Represents the cross position types.

Enum Members

Enum Member Enum Member Description
Centered
Overlap
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.