CloseRangeVisibilityBuilderPositionPaths Enumeration

NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilder.PositionPaths is an alias for NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderPositionPaths

class NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderPositionPaths

Bases: object

This enum represents the cylinder position path options.

Enum Members

Enum Member Enum Member Description
BaseData
Base data
VehicleObject
Vehicle object
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.