BaseDataPassengerBuilderSeatDirectionOptions Enumeration¶
NXOpen.Features.VehicleDesign.BaseDataPassengerBuilder.SeatDirectionOptions is an alias for NXOpen.Features.VehicleDesign.BaseDataPassengerBuilderSeatDirectionOptions
-
class
NXOpen.Features.VehicleDesign.
BaseDataPassengerBuilderSeatDirectionOptions
¶ Bases:
object
This enum represents the options to define the passenger’s seat direction type.
Enum Members
Enum Member Enum Member Description Frontward Seat position driving directionBackward Seat position opposite to the driving directionLeft Seat directed towards the left side of the car.Right Seat directed towards the right side of the car.Custom Specify a custom value for the seat position (in deg). 1 to 179: Turning the seat rightwards; 1 to 179: Turning the seat leftwards.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-