BaseDataLoadingBuilderLoadingType Enumeration

NXOpen.Features.VehicleDesign.BaseDataLoadingBuilder.LoadingType is an alias for NXOpen.Features.VehicleDesign.BaseDataLoadingBuilderLoadingType

class NXOpen.Features.VehicleDesign.BaseDataLoadingBuilderLoadingType

Bases: object

This enum represents the vehicle loading types.

Enum Members

Enum Member Enum Member Description
Standard
Standard - Defined in the registration file, user can not delete it.
UserDefined
User-Defined - user can add or delete it.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.