VariableRadiusPointsBuilder Class¶
-
class
NXOpen.Features.
VariableRadiusPointsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.VariableRadiusPointsBuilder
builderTo create a new instance of this class, use
NXOpen.Features.FlowBlendBuilder.NewControlPoint()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Location | Returns or sets the location of variable radius point |
Radius | Returns the radius of variable radius point |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Location¶
-
VariableRadiusPointsBuilder.
Location
¶ Returns or sets the location of variable radius point
-------------------------------------
Getter Method
Signature
Location()
Returns: Return type: NXOpen.Point
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Location(location)
Parameters: location ( NXOpen.Point
) –New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Radius¶
-
VariableRadiusPointsBuilder.
Radius
¶ Returns the radius of variable radius point
-------------------------------------
Getter Method
Signature
Radius()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
VariableRadiusPointsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.