VariableOffsetBuilderMethodOptions Enumeration

NXOpen.Features.VariableOffsetBuilder.MethodOptions is an alias for NXOpen.Features.VariableOffsetBuilderMethodOptions

class NXOpen.Features.VariableOffsetBuilderMethodOptions

Bases: object

offset methods for creating the new surface

Enum Members

Enum Member Enum Member Description
Linear
linear offset applied along both of U and V directions
Cubic
cublic offset applied along both of U and V directions
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.