VarOffsetFaceBuilder Class¶
-
class
NXOpen.Features.
VarOffsetFaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
Features.VarOffsetFace
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateVarOffsetFaceBuilder()
Default values.
Property Value BodyOutput OffsetasNewBody BridgeContinuity Connected New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
BodyOutput | Returns or sets the body output |
BoundaryObject | Returns the boundary object |
BridgeContinuity | Returns or sets the bridge continuity |
OffsetDirection | Returns or sets the offset direction |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProjectionDirection | Returns the projection direction |
RegionList | Returns the region list |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetFace | Returns the target face |
Type | Returns or sets the type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreateRegionListItem | The region selection type dim object’s create function @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ErasePointBoundaryMap | Erase the key value from region point - boundary map |
ErasePointLaminarMap | Erase the key value from region point - laminar edges map |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
InsertPointBoundaryMap | Insert to region point - boundary map |
InsertPointLaminarMap | Insert to region point - laminar edges map |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
VarOffsetFaceBuilderContinuity Enumeration | bridge continuity |
VarOffsetFaceBuilderOutput Enumeration | body output type |
VarOffsetFaceBuilderTypes Enumeration | feature type |
Property Detail¶
BodyOutput¶
-
VarOffsetFaceBuilder.
BodyOutput
¶ Returns or sets the body output
-------------------------------------
Getter Method
Signature
BodyOutput()
Returns: Return type: NXOpen.Features.VarOffsetFaceBuilderOutput
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BodyOutput(bodyOutput)
Parameters: bodyOutput ( NXOpen.Features.VarOffsetFaceBuilderOutput
) –New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
BoundaryObject¶
-
VarOffsetFaceBuilder.
BoundaryObject
¶ Returns the boundary object
-------------------------------------
Getter Method
Signature
BoundaryObject()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX11.0.0.
License requirements: None.
BridgeContinuity¶
-
VarOffsetFaceBuilder.
BridgeContinuity
¶ Returns or sets the bridge continuity
-------------------------------------
Getter Method
Signature
BridgeContinuity()
Returns: Return type: NXOpen.Features.VarOffsetFaceBuilderContinuity
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BridgeContinuity(bridgeContinuity)
Parameters: bridgeContinuity ( NXOpen.Features.VarOffsetFaceBuilderContinuity
) –New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
OffsetDirection¶
-
VarOffsetFaceBuilder.
OffsetDirection
¶ Returns or sets the offset direction
-------------------------------------
Getter Method
Signature
OffsetDirection()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetDirection(offsetDirection)
Parameters: offsetDirection (bool) – New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProjectionDirection¶
-
VarOffsetFaceBuilder.
ProjectionDirection
¶ Returns the projection direction
-------------------------------------
Getter Method
Signature
ProjectionDirection()
Returns: Projection Options data Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX11.0.0.
License requirements: None.
RegionList¶
-
VarOffsetFaceBuilder.
RegionList
¶ Returns the region list
-------------------------------------
Getter Method
Signature
RegionList()
Returns: Return type: NXOpen.Features.RegionListItemBuilderList
New in version NX11.0.0.
License requirements: None.
TargetFace¶
-
VarOffsetFaceBuilder.
TargetFace
¶ Returns the target face
-------------------------------------
Getter Method
Signature
TargetFace()
Returns: Return type: NXOpen.ScCollector
New in version NX11.0.0.
License requirements: None.
Type¶
-
VarOffsetFaceBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.VarOffsetFaceBuilderTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.VarOffsetFaceBuilderTypes
) –New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
CreateRegionListItem¶
-
VarOffsetFaceBuilder.
CreateRegionListItem
¶ The region selection type dim object’s create function
Signature
CreateRegionListItem()
Returns: Return type: NXOpen.Features.RegionListItemBuilder
New in version NX11.0.0.
License requirements: None.
ErasePointBoundaryMap¶
-
VarOffsetFaceBuilder.
ErasePointBoundaryMap
¶ Erase the key value from region point - boundary map
Signature
ErasePointBoundaryMap(regionPoint)
Parameters: regionPoint ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ErasePointLaminarMap¶
-
VarOffsetFaceBuilder.
ErasePointLaminarMap
¶ Erase the key value from region point - laminar edges map
Signature
ErasePointLaminarMap(regionPoint)
Parameters: regionPoint ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InsertPointBoundaryMap¶
-
VarOffsetFaceBuilder.
InsertPointBoundaryMap
¶ Insert to region point - boundary map
Signature
InsertPointBoundaryMap(regionPoint, regionBoundaries)
Parameters: - regionPoint (
NXOpen.NXObject
) – - regionBoundaries (list of
NXOpen.NXObject
) –
New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
- regionPoint (
InsertPointLaminarMap¶
-
VarOffsetFaceBuilder.
InsertPointLaminarMap
¶ Insert to region point - laminar edges map
Signature
InsertPointLaminarMap(regionPoint, regionLaminarEdges)
Parameters: - regionPoint (
NXOpen.NXObject
) – - regionLaminarEdges (list of
NXOpen.NXObject
) –
New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
- regionPoint (
Validate¶
-
VarOffsetFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.