UserDefinedFeatureIconEvent Class

class NXOpen.Features.UserDefinedFeatureIconEvent

Bases: NXOpen.TaggedObject

JA interface for the UserDefinedFeatureIconEvent object

This calls cannot be created

New in version NX8.0.0.

Properties

Property Description
ClassName Returns the class name
IconName Returns or sets the icon name
Instantiation Returns the UDF instantiation feature
Tag Returns the Tag for this object.

Methods

Property Detail

ClassName

UserDefinedFeatureIconEvent.ClassName

Returns the class name

-------------------------------------

Getter Method

Signature ClassName()

Returns:
Return type:str

New in version NX8.0.0.

License requirements: None.

IconName

UserDefinedFeatureIconEvent.IconName

Returns or sets the icon name

-------------------------------------

Getter Method

Signature IconName()

Returns:
Return type:str

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature IconName(className)

Parameters:className (str) –

New in version NX8.0.0.

License requirements: None.

Instantiation

UserDefinedFeatureIconEvent.Instantiation

Returns the UDF instantiation feature

-------------------------------------

Getter Method

Signature Instantiation()

Returns:The UDF instantiation feature
Return type:NXOpen.Features.Feature

New in version NX8.0.0.

License requirements: None.