UserDefinedFeatureEditEvent Class

class NXOpen.Features.UserDefinedFeatureEditEvent

Bases: NXOpen.TaggedObject

JA interface for the UserDefinedFeatureEditEvent object

This calls cannot be created

New in version NX8.0.0.

Properties

Property Description
ClassName Returns the class name
Feature Returns the related UDF
Response Returns or sets the response
Tag Returns the Tag for this object.

Methods

Property Detail

ClassName

UserDefinedFeatureEditEvent.ClassName

Returns the class name

-------------------------------------

Getter Method

Signature ClassName()

Returns:
Return type:str

New in version NX8.0.0.

License requirements: None.

Feature

UserDefinedFeatureEditEvent.Feature

Returns the related UDF

-------------------------------------

Getter Method

Signature Feature()

Returns:The UDF that caused the event to fire
Return type:NXOpen.Features.Feature

New in version NX8.0.0.

License requirements: None.

Response

UserDefinedFeatureEditEvent.Response

Returns or sets the response

-------------------------------------

Getter Method

Signature Response()

Returns:
Return type:int

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Response(response)

Parameters:response (int) –

New in version NX8.0.0.

License requirements: None.