UserDefinedFeatureClass Class

class NXOpen.Features.UserDefinedFeatureClass

Bases: NXOpen.TransientObject

JA interface for UserDefinedFeatureClass

An instance of this class can be obtained from Features.UserDefinedFeatureClassManager.CreateClass()

New in version NX8.0.0.

Properties

Property Description
ClassName Returns the class name

Methods

Method Description
AddCopyHandler Registers the copy callback.
AddCreateHandler Registers the create callback.
AddEditHandler Registers the edit callback.
AddIconHandler Registers the udf icon callback.
AddUpdateHandler Registers the udf update callback.
Dispose Frees the memory associated with this object.

Property Detail

ClassName

UserDefinedFeatureClass.ClassName

Returns the class name

-------------------------------------

Getter Method

Signature ClassName()

Returns:the class name
Return type:str

New in version NX8.0.0.

License requirements: None.

Method Detail

AddCopyHandler

UserDefinedFeatureClass.AddCopyHandler

Registers the copy callback.

Signature AddCopyHandler(copyCallback)

Parameters:copyCallback (CallableObject) –

New in version NX8.0.0.

License requirements: None.

AddCreateHandler

UserDefinedFeatureClass.AddCreateHandler

Registers the create callback.

Signature AddCreateHandler(createCallback)

Parameters:createCallback (CallableObject) –

New in version NX8.0.0.

License requirements: None.

AddEditHandler

UserDefinedFeatureClass.AddEditHandler

Registers the edit callback.

Signature AddEditHandler(editCallback)

Parameters:editCallback (CallableObject) –

New in version NX8.0.0.

License requirements: None.

AddIconHandler

UserDefinedFeatureClass.AddIconHandler

Registers the udf icon callback.

Signature AddIconHandler(iconCallback)

Parameters:iconCallback (CallableObject) –

New in version NX8.0.0.

License requirements: None.

AddUpdateHandler

UserDefinedFeatureClass.AddUpdateHandler

Registers the udf update callback.

Signature AddUpdateHandler(updateCallback)

Parameters:updateCallback (CallableObject) –

New in version NX8.0.0.

License requirements: None.

Dispose

UserDefinedFeatureClass.Dispose

Frees the memory associated with this object.

After invocation of this method, the object is no longer valid.

Signature Dispose()

New in version NX8.0.0.

License requirements: None.