UnsewBuilderUnsewOutput Enumeration

NXOpen.Features.UnsewBuilder.UnsewOutput is an alias for NXOpen.Features.UnsewBuilderUnsewOutput

class NXOpen.Features.UnsewBuilderUnsewOutput

Bases: object

Unsew body option type.

Enum Members

Enum Member Enum Member Description
OneBodyForConnectedFaces
One body for connected unsewn faces
OneBodyForEachFace
One body for every unsewn face.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.