TubeBuilderOutput Enumeration

NXOpen.Features.TubeBuilder.Output is an alias for NXOpen.Features.TubeBuilderOutput

class NXOpen.Features.TubeBuilderOutput

Bases: object

This enum represents the topology output option

Enum Members

Enum Member Enum Member Description
MultipleSegments
multiple segments output
SingleSegment
single segment output
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.