TrimSheetBuilder Class¶
-
class
NXOpen.Features.
TrimSheetBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.TrimSheet
builder.Inputs to this class can be convergent objects.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateTrimsheetBuilder()
Default values.
Property Value ImprintBothSide True KeepDiscardMethod Keep New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AllowTargetEdgesAsToolObjects | Returns or sets the allow target edges as tool objects |
ApplyToCopyOfSheets | Returns or sets the apply to copy of sheets |
BoundaryObjects | Returns the boundry objects |
ExtendBoundaryObject | Returns or sets the extend boundary object to target laminar edges |
ImprintBothSide | Returns or sets the imprint both side |
KeepDiscardMethod | Returns or sets the keep discard method |
OutputExactGeometry | Returns or sets the output exact geometry |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProjectionDirection | Returns the projection direction |
Regions | Returns the regions |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetBodies | Returns the target bodies |
Tolerance | Returns or sets the tolerance |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TrimSheetBuilderKeepDiscardOption Enumeration | Represents the keep discard options for selected region |
Property Detail¶
AllowTargetEdgesAsToolObjects¶
-
TrimSheetBuilder.
AllowTargetEdgesAsToolObjects
¶ Returns or sets the allow target edges as tool objects
-------------------------------------
Getter Method
Signature
AllowTargetEdgesAsToolObjects()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllowTargetEdgesAsToolObjects(allowTargetEdgesAsToolObjects)
Parameters: allowTargetEdgesAsToolObjects (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ApplyToCopyOfSheets¶
-
TrimSheetBuilder.
ApplyToCopyOfSheets
¶ Returns or sets the apply to copy of sheets
-------------------------------------
Getter Method
Signature
ApplyToCopyOfSheets()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplyToCopyOfSheets(applyToCopyOfSheets)
Parameters: applyToCopyOfSheets (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
BoundaryObjects¶
-
TrimSheetBuilder.
BoundaryObjects
¶ Returns the boundry objects
-------------------------------------
Getter Method
Signature
BoundaryObjects()
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
License requirements: None.
ExtendBoundaryObject¶
-
TrimSheetBuilder.
ExtendBoundaryObject
¶ Returns or sets the extend boundary object to target laminar edges
-------------------------------------
Getter Method
Signature
ExtendBoundaryObject()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendBoundaryObject(extendBoundaryObject)
Parameters: extendBoundaryObject (bool) – New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ImprintBothSide¶
-
TrimSheetBuilder.
ImprintBothSide
¶ Returns or sets the imprint both side
-------------------------------------
Getter Method
Signature
ImprintBothSide()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImprintBothSide(imprintBothSide)
Parameters: imprintBothSide (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
KeepDiscardMethod¶
-
TrimSheetBuilder.
KeepDiscardMethod
¶ Returns or sets the keep discard method
-------------------------------------
Getter Method
Signature
KeepDiscardMethod()
Returns: Return type: NXOpen.Features.TrimSheetBuilderKeepDiscardOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepDiscardMethod(keepDiscardMethod)
Parameters: keepDiscardMethod ( NXOpen.Features.TrimSheetBuilderKeepDiscardOption
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OutputExactGeometry¶
-
TrimSheetBuilder.
OutputExactGeometry
¶ Returns or sets the output exact geometry
-------------------------------------
Getter Method
Signature
OutputExactGeometry()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputExactGeometry(outputExactGeometry)
Parameters: outputExactGeometry (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ProjectionDirection¶
-
TrimSheetBuilder.
ProjectionDirection
¶ Returns the projection direction
-------------------------------------
Getter Method
Signature
ProjectionDirection()
Returns: Projection Options data Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX5.0.0.
License requirements: None.
Regions¶
-
TrimSheetBuilder.
Regions
¶ Returns the regions
-------------------------------------
Getter Method
Signature
Regions()
Returns: Return type: NXOpen.RegionPointList
New in version NX5.0.0.
License requirements: None.
TargetBodies¶
-
TrimSheetBuilder.
TargetBodies
¶ Returns the target bodies
-------------------------------------
Getter Method
Signature
TargetBodies()
Returns: Return type: NXOpen.SelectBodyList
New in version NX5.0.0.
License requirements: None.
Tolerance¶
-
TrimSheetBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
TrimSheetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.