TrimExtendBuilderArrowSideOptions Enumeration

NXOpen.Features.TrimExtendBuilder.ArrowSideOptions is an alias for NXOpen.Features.TrimExtendBuilderArrowSideOptions

class NXOpen.Features.TrimExtendBuilderArrowSideOptions

Bases: object

This enum represents the TrimExtend Arrow Side Options

Enum Members

Enum Member Enum Member Description
Retain
Retain
Delete
Delete
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.