ThroughCurvesBuilderPatchTypes Enumeration

NXOpen.Features.ThroughCurvesBuilder.PatchTypes is an alias for NXOpen.Features.ThroughCurvesBuilderPatchTypes

class NXOpen.Features.ThroughCurvesBuilderPatchTypes

Bases: object

This enum represents the Patch options.

Enum Members

Enum Member Enum Member Description
Single
single patch.
Multiple
multiple patches.
MatchString
patch match string.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.