ThroughCurvesBuilderConstructionMethod Enumeration

NXOpen.Features.ThroughCurvesBuilder.ConstructionMethod is an alias for NXOpen.Features.ThroughCurvesBuilderConstructionMethod

class NXOpen.Features.ThroughCurvesBuilderConstructionMethod

Bases: object

This enum represents the Construction options.

Enum Members

Enum Member Enum Member Description
Normal
Use the standard procedures.
SplinePoints
Use the points and tangent values at the points for reparameterizing curves.
Simple
Build the simplest mesh surface possible.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.