TextBuilderOrientationMethodOptions Enumeration¶
NXOpen.Features.TextBuilder.OrientationMethodOptions is an alias for NXOpen.Features.TextBuilderOrientationMethodOptions
-
class
NXOpen.Features.
TextBuilderOrientationMethodOptions
¶ Bases:
object
The orientation options for
NXOpen.Features.TextBuilderTypes.OnCurve
typeEnum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “Natural”, ” Orientation along natural curve normals ” “Vector”, ” Orientation along a vector “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.