TextBuilderOnFacePlacementMethodOptions Enumeration¶
NXOpen.Features.TextBuilder.OnFacePlacementMethodOptions is an alias for NXOpen.Features.TextBuilderOnFacePlacementMethodOptions
-
class
NXOpen.Features.
TextBuilderOnFacePlacementMethodOptions
¶ Bases:
object
The placement options for
NXOpen.Features.TextBuilderTypes.OnFace
typeEnum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “CurvesOnFaces”, ” Placement on curves or edges on the faces ” “SectionPlane”, ” Placement on intersection curve created by a plane and the faces “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.