TabNoteCfgBuilderRefplane Enumeration

NXOpen.Features.TabNoteCfgBuilder.Refplane is an alias for NXOpen.Features.TabNoteCfgBuilderRefplane

class NXOpen.Features.TabNoteCfgBuilderRefplane

Bases: object

the reference plane type.

Enum Members

Enum Member Enum Member Description
Xy
0 : Xc-Yc plane
Yz
1 : Yc-Zc plane
Zx
2 : Zc-Xc plane
NegXy
3 : - Xc-Yc plane
NegYz
4 : - Yc-Zc plane
NegZx
5 : - Zc-Xc plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.