SweptBuilderSectionLocationTypes Enumeration

NXOpen.Features.SweptBuilder.SectionLocationTypes is an alias for NXOpen.Features.SweptBuilderSectionLocationTypes

class NXOpen.Features.SweptBuilderSectionLocationTypes

Bases: object

This enum represents the Section Location option.

If a single section located at the middle of a guide string is specified, Anywhere Along Guides option sweeps in both directions.

Enum Members

Enum Member Enum Member Description
AnywhereAlongGuides
Anywhere along Guides
EndsOfGuides
Ends of Guides
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.