SweptBuilderInterpolationOptions Enumeration

NXOpen.Features.SweptBuilder.InterpolationOptions is an alias for NXOpen.Features.SweptBuilderInterpolationOptions

class NXOpen.Features.SweptBuilderInterpolationOptions

Bases: object

This enum represents the Interpolation option.

For 2 or more sections, this option specifies the method by which to interpolate between them, either Linear or Cubic.

Enum Members

Enum Member Enum Member Description
Linear
Linear
Cubic
Cubic
Blend
Blend
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.