SubdivisionSubdivideFaceBuilder Class¶
-
class
NXOpen.Features.Subdivision.
SubdivisionSubdivideFaceBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.Subdivision.SubdivisionSubdivideFaceBuilder
builder.To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateSubdivisionSubdivideFaceBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
FacesToSubdivide | Returns the faces to subdivide. |
Scale | Returns the scale factor. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Subdivide | Perform subdivide operation. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FacesToSubdivide¶
-
SubdivisionSubdivideFaceBuilder.
FacesToSubdivide
¶ Returns the faces to subdivide.
-------------------------------------
Getter Method
Signature
FacesToSubdivide()
Returns: Return type: NXOpen.Features.Subdivision.SelectCageObjectData
New in version NX9.0.0.
License requirements: None.
Scale¶
-
SubdivisionSubdivideFaceBuilder.
Scale
¶ Returns the scale factor.
The value is from 0 to 100. 0 refers to the original size of the face, 100 refers to the center of the face.
-------------------------------------
Getter Method
Signature
Scale()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Subdivide¶
-
SubdivisionSubdivideFaceBuilder.
Subdivide
¶ Perform subdivide operation.
Signature
Subdivide()
New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Validate¶
-
SubdivisionSubdivideFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.