SubdivisionProjectCageBuilderTypes Enumeration

NXOpen.Features.Subdivision.SubdivisionProjectCageBuilder.Types is an alias for NXOpen.Features.Subdivision.SubdivisionProjectCageBuilderTypes

class NXOpen.Features.Subdivision.SubdivisionProjectCageBuilderTypes

Bases: object

The type of projection

Enum Members

Enum Member Enum Member Description
ToTarget
Project on target
ToAverage
Project using best fit plane or axis
AlignNormal
Align edges normal to the specified plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.