SubdivisionPrimitiveShapeBuilderEx Class¶
-
class
NXOpen.Features.Subdivision.
SubdivisionPrimitiveShapeBuilderEx
¶ Bases:
NXOpen.Builder
Represents a
Features.Subdivision.SubdivisionPrimitiveShapeBuilderEx
builder.To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateSubdivisionPrimitiveShapeBuilderEx()
Default values.
Property Value CircularSegments 4 Height.Value 100 (millimeters part), 4 (inches part) HeightZ.Value 100 (millimeters part), 4 (inches part) InnerSize.Value 50 (millimeters part), 2 (inches part) LengthX.Value 100 (millimeters part), 4 (inches part) LinearSegments 1 OuterSize.Value 100 (millimeters part), 4 (inches part) RadialSegments 8 Size.Value 100 (millimeters part), 4 (inches part) WidthY.Value 100 (millimeters part), 4 (inches part) XSegments 1 YSegments 1 ZSegments 1 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CircularSegments | Returns or sets the number of segments in circular direction. |
Height | Returns the height. |
HeightZ | Returns the height in Z direction. |
InnerSize | Returns the inner size of torus. |
LengthX | Returns the length in X direction. |
LinearSegments | Returns or sets the number of segments in linear direction. |
Origin | Returns or sets the origin. |
OuterSize | Returns the outer size of torus. |
RadialSegments | Returns or sets the number of segments in radial direction. |
Size | Returns the size. |
SphereSubdivisionLevelOption | Returns or sets the subdivision level. |
Tag | Returns the Tag for this object. |
Transformer | Returns the transformation tool. |
Type | Returns or sets the type. |
WidthY | Returns the width in Y direction. |
XSegments | Returns or sets the number of segments in X direction. |
YSegments | Returns or sets the number of segments in Y direction. |
ZSegments | Returns or sets the number of segments in Z direction. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateMesh | Updates the mesh data after changes in the origin. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SubdivisionPrimitiveShapeBuilderExSphereSubdivisionLevel Enumeration | Level of subdivisions of cubical cage to construct spherical primitive. |
SubdivisionPrimitiveShapeBuilderExTypes Enumeration | Type of primitive. |
Property Detail¶
CircularSegments¶
-
SubdivisionPrimitiveShapeBuilderEx.
CircularSegments
¶ Returns or sets the number of segments in circular direction.
-------------------------------------
Getter Method
Signature
CircularSegments()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CircularSegments(numSegments)
Parameters: numSegments (int) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Height¶
-
SubdivisionPrimitiveShapeBuilderEx.
Height
¶ Returns the height.
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
HeightZ¶
-
SubdivisionPrimitiveShapeBuilderEx.
HeightZ
¶ Returns the height in Z direction.
-------------------------------------
Getter Method
Signature
HeightZ()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
InnerSize¶
-
SubdivisionPrimitiveShapeBuilderEx.
InnerSize
¶ Returns the inner size of torus.
-------------------------------------
Getter Method
Signature
InnerSize()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
LengthX¶
-
SubdivisionPrimitiveShapeBuilderEx.
LengthX
¶ Returns the length in X direction.
-------------------------------------
Getter Method
Signature
LengthX()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
LinearSegments¶
-
SubdivisionPrimitiveShapeBuilderEx.
LinearSegments
¶ Returns or sets the number of segments in linear direction.
-------------------------------------
Getter Method
Signature
LinearSegments()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinearSegments(numSegments)
Parameters: numSegments (int) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Origin¶
-
SubdivisionPrimitiveShapeBuilderEx.
Origin
¶ Returns or sets the origin.
-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Origin(origin)
Parameters: origin ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
OuterSize¶
-
SubdivisionPrimitiveShapeBuilderEx.
OuterSize
¶ Returns the outer size of torus.
-------------------------------------
Getter Method
Signature
OuterSize()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
RadialSegments¶
-
SubdivisionPrimitiveShapeBuilderEx.
RadialSegments
¶ Returns or sets the number of segments in radial direction.
-------------------------------------
Getter Method
Signature
RadialSegments()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialSegments(numSegments)
Parameters: numSegments (int) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Size¶
-
SubdivisionPrimitiveShapeBuilderEx.
Size
¶ Returns the size.
-------------------------------------
Getter Method
Signature
Size()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
SphereSubdivisionLevelOption¶
-
SubdivisionPrimitiveShapeBuilderEx.
SphereSubdivisionLevelOption
¶ Returns or sets the subdivision level.
-------------------------------------
Getter Method
Signature
SphereSubdivisionLevelOption()
Returns: Return type: NXOpen.Features.Subdivision.SubdivisionPrimitiveShapeBuilderExSphereSubdivisionLevel
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SphereSubdivisionLevelOption(level)
Parameters: level ( NXOpen.Features.Subdivision.SubdivisionPrimitiveShapeBuilderExSphereSubdivisionLevel
) –New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Transformer¶
-
SubdivisionPrimitiveShapeBuilderEx.
Transformer
¶ Returns the transformation tool.
-------------------------------------
Getter Method
Signature
Transformer()
Returns: Return type: NXOpen.GeometricUtilities.TransformerData
New in version NX11.0.0.
License requirements: None.
Type¶
-
SubdivisionPrimitiveShapeBuilderEx.
Type
¶ Returns or sets the type.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.Subdivision.SubdivisionPrimitiveShapeBuilderExTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.Subdivision.SubdivisionPrimitiveShapeBuilderExTypes
) –New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
WidthY¶
-
SubdivisionPrimitiveShapeBuilderEx.
WidthY
¶ Returns the width in Y direction.
-------------------------------------
Getter Method
Signature
WidthY()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
XSegments¶
-
SubdivisionPrimitiveShapeBuilderEx.
XSegments
¶ Returns or sets the number of segments in X direction.
-------------------------------------
Getter Method
Signature
XSegments()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XSegments(numSegments)
Parameters: numSegments (int) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
YSegments¶
-
SubdivisionPrimitiveShapeBuilderEx.
YSegments
¶ Returns or sets the number of segments in Y direction.
-------------------------------------
Getter Method
Signature
YSegments()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YSegments(numSegments)
Parameters: numSegments (int) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
ZSegments¶
-
SubdivisionPrimitiveShapeBuilderEx.
ZSegments
¶ Returns or sets the number of segments in Z direction.
-------------------------------------
Getter Method
Signature
ZSegments()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZSegments(numSegments)
Parameters: numSegments (int) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Method Detail¶
UpdateMesh¶
-
SubdivisionPrimitiveShapeBuilderEx.
UpdateMesh
¶ Updates the mesh data after changes in the origin.
Signature
UpdateMesh()
New in version NX11.0.0.
License requirements: None.
Validate¶
-
SubdivisionPrimitiveShapeBuilderEx.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.