SubdivisionExtrudeCageBuilder Class¶
-
class
NXOpen.Features.Subdivision.
SubdivisionExtrudeCageBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilder
builder.To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateSubdivisionExtrudeCageBuilder()
Default values.
Property Value CanRelocateToolToSelection true CanReorientToolToSelection true NumberOfSegments 1 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CanMoveToolOnly | Returns or sets the flag indicating if transformer tool can be moved without transforming the selected cage topology. |
CanRelocateToolToSelection | Returns or sets the flag indicating if transformer tool can be relocated based on cage topology selection. |
CanReorientToolToSelection | Returns or sets the flag indicating if transformer tool can be reoriented based on cage topology selection. |
Continuity | Returns or sets the continuity. |
DirectionOption | Returns or sets the direction option |
Distance | Returns the distance. |
NumberOfSegments | Returns or sets the number of segments. |
ScalingMethod | Returns or sets the scaling method. |
SelectionObject | Returns the selection object. |
Tag | Returns the Tag for this object. |
TransformationMethod | Returns or sets the transformation method. |
Transformer | Returns the transformation tool. |
Vector | Returns or sets the vector for extrude. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
Extrude | Perform extrude operation. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SubdivisionExtrudeCageBuilderContinuityType Enumeration | Type of continuity. |
SubdivisionExtrudeCageBuilderDirectionType Enumeration | Represents the extrude direction. |
SubdivisionExtrudeCageBuilderScalingMethodType Enumeration | Scaling method |
SubdivisionExtrudeCageBuilderTransformationMethodType Enumeration | Transformation method types |
Property Detail¶
CanMoveToolOnly¶
-
SubdivisionExtrudeCageBuilder.
CanMoveToolOnly
¶ Returns or sets the flag indicating if transformer tool can be moved without transforming the selected cage topology.
-------------------------------------
Getter Method
Signature
CanMoveToolOnly()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanMoveToolOnly(canMove)
Parameters: canMove (bool) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
CanRelocateToolToSelection¶
-
SubdivisionExtrudeCageBuilder.
CanRelocateToolToSelection
¶ Returns or sets the flag indicating if transformer tool can be relocated based on cage topology selection.
-------------------------------------
Getter Method
Signature
CanRelocateToolToSelection()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanRelocateToolToSelection(canRelocate)
Parameters: canRelocate (bool) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
CanReorientToolToSelection¶
-
SubdivisionExtrudeCageBuilder.
CanReorientToolToSelection
¶ Returns or sets the flag indicating if transformer tool can be reoriented based on cage topology selection.
-------------------------------------
Getter Method
Signature
CanReorientToolToSelection()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanReorientToolToSelection(canReorient)
Parameters: canReorient (bool) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Continuity¶
-
SubdivisionExtrudeCageBuilder.
Continuity
¶ Returns or sets the continuity.
The continuity is used to specify creases in the limit surface corresponding to the outer edges of the faces or boundary edges specified by
NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilder.SelectionObject`()
.-------------------------------------
Getter Method
Signature
Continuity()
Returns: Return type: NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilderContinuityType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Continuity(continuity)
Parameters: continuity ( NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilderContinuityType
) –New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
DirectionOption¶
-
SubdivisionExtrudeCageBuilder.
DirectionOption
¶ Returns or sets the direction option
-------------------------------------
Getter Method
Signature
DirectionOption()
Returns: Return type: NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilderDirectionType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionOption(directionOption)
Parameters: directionOption ( NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilderDirectionType
) –New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Distance¶
-
SubdivisionExtrudeCageBuilder.
Distance
¶ Returns the distance.
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
NumberOfSegments¶
-
SubdivisionExtrudeCageBuilder.
NumberOfSegments
¶ Returns or sets the number of segments.
-------------------------------------
Getter Method
Signature
NumberOfSegments()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfSegments(numOfSegments)
Parameters: numOfSegments (int) – New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
ScalingMethod¶
-
SubdivisionExtrudeCageBuilder.
ScalingMethod
¶ Returns or sets the scaling method.
-------------------------------------
Getter Method
Signature
ScalingMethod()
Returns: Return type: NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilderScalingMethodType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingMethod(scalingMethod)
Parameters: scalingMethod ( NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilderScalingMethodType
) –New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
SelectionObject¶
-
SubdivisionExtrudeCageBuilder.
SelectionObject
¶ Returns the selection object.
-------------------------------------
Getter Method
Signature
SelectionObject()
Returns: Return type: NXOpen.Features.Subdivision.SelectCageObjectData
New in version NX9.0.0.
License requirements: None.
TransformationMethod¶
-
SubdivisionExtrudeCageBuilder.
TransformationMethod
¶ Returns or sets the transformation method.
-------------------------------------
Getter Method
Signature
TransformationMethod()
Returns: Return type: NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilderTransformationMethodType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransformationMethod(method)
Parameters: method ( NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilderTransformationMethodType
) –New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Transformer¶
-
SubdivisionExtrudeCageBuilder.
Transformer
¶ Returns the transformation tool.
-------------------------------------
Getter Method
Signature
Transformer()
Returns: Return type: NXOpen.GeometricUtilities.TransformerData
New in version NX11.0.0.
License requirements: None.
Vector¶
-
SubdivisionExtrudeCageBuilder.
Vector
¶ Returns or sets the vector for extrude.
-------------------------------------
Getter Method
Signature
Vector()
Returns: Return type: NXOpen.Direction
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector(vector)
Parameters: vector ( NXOpen.Direction
) –New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Method Detail¶
Extrude¶
-
SubdivisionExtrudeCageBuilder.
Extrude
¶ Perform extrude operation.
Signature
Extrude()
New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Validate¶
-
SubdivisionExtrudeCageBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.