StartSymmetricModelingBuilderMirrorProcedureOption Enumeration

NXOpen.Features.Subdivision.StartSymmetricModelingBuilder.MirrorProcedureOption is an alias for NXOpen.Features.Subdivision.StartSymmetricModelingBuilderMirrorProcedureOption

class NXOpen.Features.Subdivision.StartSymmetricModelingBuilderMirrorProcedureOption

Bases: object

The options used to establish symmetric model

Deprecated since version NX10.0.0: This enumeration is redundent and hence not necessary.

Enum Members

Enum Member Enum Member Description
CutBody
Cuts the mesh
ProjectEdge
Projects the edges
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.