SplitSubdivisionBodyBuilderInputBodyOptions Enumeration¶
NXOpen.Features.Subdivision.SplitSubdivisionBodyBuilder.InputBodyOptions is an alias for NXOpen.Features.Subdivision.SplitSubdivisionBodyBuilderInputBodyOptions
-
class
NXOpen.Features.Subdivision.
SplitSubdivisionBodyBuilderInputBodyOptions
¶ Bases:
object
Options indicating actions to be taken on input
Features.Subdivision.SubdivisionBody
featuresEnum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “Keep”, ” Keep the feature as they are ” “Hide”, ” Hide the features ” “Delete”, ” Delete the features “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.