ExtractCagePolylineBuilderInputCurveOption Enumeration

NXOpen.Features.Subdivision.ExtractCagePolylineBuilder.InputCurveOption is an alias for NXOpen.Features.Subdivision.ExtractCagePolylineBuilderInputCurveOption

class NXOpen.Features.Subdivision.ExtractCagePolylineBuilderInputCurveOption

Bases: object

Input curves options.

Enum Members

Enum Member Enum Member Description
Keep
Keep input curves as they are
Hide
Hide input curves
Delete
Delete input curves
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.