ExportSubdivisionGeometryBuilder Class¶
-
class
NXOpen.Features.Subdivision.
ExportSubdivisionGeometryBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.Subdivision.ExportSubdivisionGeometryBuilder
builder.To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateExportSubdivisionGeometryBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
FeatureSet | Returns the Feature to export |
FileName | Returns or sets the file name. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FeatureSet¶
-
ExportSubdivisionGeometryBuilder.
FeatureSet
¶ Returns the Feature to export
-------------------------------------
Getter Method
Signature
FeatureSet()
Returns: Return type: NXOpen.Features.SelectFeatureList
New in version NX11.0.0.
License requirements: None.
FileName¶
-
ExportSubdivisionGeometryBuilder.
FileName
¶ Returns or sets the file name.
The export file will only store the topology and geometry positions of the Subdivision Cage, and not contains auxiliary data of the Subdivision feature, such as the weights, sharpness and constraints.
-------------------------------------
Getter Method
Signature
FileName()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FileName(filename)
Parameters: filename (str) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Method Detail¶
Validate¶
-
ExportSubdivisionGeometryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.