DefineWorkRegionBuilder Class¶
-
class
NXOpen.Features.Subdivision.
DefineWorkRegionBuilder
¶ Bases:
NXOpen.Builder
Represents a
Features.Subdivision.DefineWorkRegionBuilder
builder.To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateDefineWorkRegionBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
FrozenColor | Returns or sets the frozen region color |
FrozenRegionDefinitionMethod | Returns or sets the frozen region method |
Tag | Returns the Tag for this object. |
WorkRegionDefinitionMethod | Returns or sets the work region definition method |
WorkRegionObjects | Returns the work region objects |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DefineWorkRegionBuilderFrozenRegionDefinitionMethods Enumeration | Method of defining frozen region. |
DefineWorkRegionBuilderWorkRegionDefinitionMethods Enumeration | Method of defining work region. |
Property Detail¶
FrozenColor¶
-
DefineWorkRegionBuilder.
FrozenColor
¶ Returns or sets the frozen region color
-------------------------------------
Getter Method
Signature
FrozenColor()
Returns: Return type: Id New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrozenColor(frozenColor)
Parameters: frozenColor (Id) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
FrozenRegionDefinitionMethod¶
-
DefineWorkRegionBuilder.
FrozenRegionDefinitionMethod
¶ Returns or sets the frozen region method
-------------------------------------
Getter Method
Signature
FrozenRegionDefinitionMethod()
Returns: Return type: NXOpen.Features.Subdivision.DefineWorkRegionBuilderFrozenRegionDefinitionMethods
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrozenRegionDefinitionMethod(frozenRegionDefinitionMethod)
Parameters: frozenRegionDefinitionMethod ( NXOpen.Features.Subdivision.DefineWorkRegionBuilderFrozenRegionDefinitionMethods
) –New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
WorkRegionDefinitionMethod¶
-
DefineWorkRegionBuilder.
WorkRegionDefinitionMethod
¶ Returns or sets the work region definition method
-------------------------------------
Getter Method
Signature
WorkRegionDefinitionMethod()
Returns: Return type: NXOpen.Features.Subdivision.DefineWorkRegionBuilderWorkRegionDefinitionMethods
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WorkRegionDefinitionMethod(workRegionDefinitionMethod)
Parameters: workRegionDefinitionMethod ( NXOpen.Features.Subdivision.DefineWorkRegionBuilderWorkRegionDefinitionMethods
) –New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
WorkRegionObjects¶
-
DefineWorkRegionBuilder.
WorkRegionObjects
¶ Returns the work region objects
-------------------------------------
Getter Method
Signature
WorkRegionObjects()
Returns: Return type: NXOpen.Features.Subdivision.SelectCageObjectData
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
DefineWorkRegionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.