CageManipulatorDataObjectSelectionData_Struct Struct¶
NXOpen.Features.Subdivision.CageManipulatorData.ObjectSelectionData is an alias for NXOpen.Features.Subdivision.CageManipulatorDataObjectSelectionData_Struct
-
class
NXOpen.Features.Subdivision.
CageManipulatorDataObjectSelectionData_Struct
¶ Bases:
object
Contains object selection information.
New in version NX9.0.0.
. Constructor: NXOpen.Features.Subdivision.CageManipulatorData.ObjectSelectionData()
Fields¶
Field | Description |
---|---|
SelectedObject | The selected object. |
SelectionPosition | The point at which object is selected, the point under the cursor when seen in view direction. |
ViewDirection | The view direction. |
IsSnappedPosition | Is SelectionPosition a snapped location. |
SelectedObject¶
-
CageManipulatorDataObjectSelectionData_Struct.
SelectedObject
¶ The selected object.
-------------------------------------
Field Value Type:
NXOpen.NXObject
SelectionPosition¶
-
CageManipulatorDataObjectSelectionData_Struct.
SelectionPosition
¶ The point at which object is selected, the point under the cursor when seen in view direction.
-------------------------------------
Field Value Type:
NXOpen.Point3d
ViewDirection¶
-
CageManipulatorDataObjectSelectionData_Struct.
ViewDirection
¶ The view direction.
-------------------------------------
Field Value Type:
NXOpen.Vector3d