StyledSweepBuilderTransitionOptions Enumeration

NXOpen.Features.StyledSweepBuilder.TransitionOptions is an alias for NXOpen.Features.StyledSweepBuilderTransitionOptions

class NXOpen.Features.StyledSweepBuilderTransitionOptions

Bases: object

This enum represents the Transition option

Enum Members

Enum Member Enum Member Description
Linear
Linear
Cubic
Cubic
Blend
Blend
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.