StyledSweepBuilderScalingMethodOptions Enumeration

NXOpen.Features.StyledSweepBuilder.ScalingMethodOptions is an alias for NXOpen.Features.StyledSweepBuilderScalingMethodOptions

class NXOpen.Features.StyledSweepBuilderScalingMethodOptions

Bases: object

This enum represents the Scaling Method option

Enum Members

Enum Member Enum Member Description
Uniform
Uniform
Nonuniform
Non-Uniform
ScalingCurve
Scaling Curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.