StyledSweepBuilderFixedStringOptions Enumeration

NXOpen.Features.StyledSweepBuilder.FixedStringOptions is an alias for NXOpen.Features.StyledSweepBuilderFixedStringOptions

class NXOpen.Features.StyledSweepBuilderFixedStringOptions

Bases: object

This enum represents the Fixed String option

Enum Members

Enum Member Enum Member Description
Guide
Guide
Section
Section
GuideAndSection
Guide and Section
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.