StyledCornerBuilderTrimCurveTypes Enumeration

NXOpen.Features.StyledCornerBuilder.TrimCurveTypes is an alias for NXOpen.Features.StyledCornerBuilderTrimCurveTypes

class NXOpen.Features.StyledCornerBuilderTrimCurveTypes

Bases: object

Trim curve types

Enum Members

Enum Member Enum Member Description
TangentContinuous
Tangent continuous type
LineProjection
Line projection type
Isoparametric
Isoparametric type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.