StyledCornerBuilderTrimAndSewMethodTypes Enumeration

NXOpen.Features.StyledCornerBuilder.TrimAndSewMethodTypes is an alias for NXOpen.Features.StyledCornerBuilderTrimAndSewMethodTypes

class NXOpen.Features.StyledCornerBuilderTrimAndSewMethodTypes

Bases: object

Trim and attach method types

Enum Members

Enum Member Enum Member Description
NoTrim
No trim
TrimBlends
Trim all blends
TrimAll
Trim blends and base wall
TrimAndAttachBlends
Trim and attach blends
TrimAndAttachAll
Trim and attach blends and base wall
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.